Tool/software:
Hi team,
Can this EVM support stand alone performance? I mean, this EVM don't have memory function and need to write SPI by GUI, right?
If so, is there any solution to use as stand alone?
Regards,
Youhei MIYAOKA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Can this EVM support stand alone performance? I mean, this EVM don't have memory function and need to write SPI by GUI, right?
If so, is there any solution to use as stand alone?
Regards,
Youhei MIYAOKA
Hello,
Thanks for your question.
In the H variant EVM, the configurations can be made from the , jumper connections. Please see the user guide and schematics for details.
Thanks,
Ibinu
Hi Ibinu,
Thanks. I understood H version can set by hardware.
By the way, is it possible to memorize setting even when EVM was shut down.
Regards,
Youhei
Hi Youhel,
Thanks for clarifying. Just to be clear can you confirm which settings needs to be memorized for the application.
Thanks,
Ibinu
Hello Miyaoka-san,
In addition to getting answers for Ibinu's question I'd like to add the present capability of the EVM for H-variant. The S-variant EVM allows Save and Load functions to save register settings for reuse.
The current architecture of the GUI SW and EVM FW does not support saving GUI settings for future use. In addition several HW settings in the EVM are made by jumper short positions which are permanent settings until you change the jumper short positions. Thank you.
Regards, Murugavel