Other Parts Discussed in Thread: MCF8316A
Tool/software:
Hello.
I am having a problem when I am debugging a brushless DC motor using the MCF8316A EVM. After I start running the motor every time, the motor speed exceeds the target speed and then drops back down to the target speed. For example, if I set it to 3600 rpm, the motor will reach 3800 rpm every time and then drop back down to 3600 rpm. If I present this effect to the customer, it will be passed over. Therefore, I would like to know if it is possible to set up a setting in motor studio so that the motor will not increase after it reaches the target speed, how do I set it up?
Sorry I'm not very good with motor studio, I would appreciate if you could guide me with pictures.