Tool/software:
Hello there,
For my application, I need to drive half bridge with 8 mosfet. Each side four mosfets are connected in parallel, each mosfet having a total gate charge of 8nC. Is it possible for me to drive the mosfets with a constant frequency of 120kHz. Is it possible to use this IC for this application? What is the maximum frequency I can achieve for this application? What is the maximum steady drive current that can be given be the gate driver IC? Any information regarding this will be helpful. Thank you.