This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8434AEVM: Technical questions

Part Number: DRV8434AEVM
Other Parts Discussed in Thread: DRV8434A, DRV8889-Q1, DRV8434-Q1, DRV8434

Tool/software:

Hi Team,

We applied DRV8434AEVM using GUI to operate the customer's motor. Customer is using 2phase 4wire motor. And we have some questions.

1. How can we measure the back-emf when motor was operating?

2. We were using DRV8434AEVM to drive customer's motor. Customer's motor was moving up and down as picture showing. Why we met stall issue when motor moved up, but no stall issue when motor moved down. (We set the same VREF)

3. When we used DRV8434AEVM, we produced the stall issue manually. But why start steps motor was still spin when stall occurred. It looks like that we didn't have stall protection, is it correct?

4. What does VREF voltage mean? Does it mean the current? May you help check if below equation is ok or not? The stepper motor spec shows the coil resistor is 8R and we use 12V. 

12/8 = 1.5A(motor current). Because we used two phase and so one phase current should be 0.75A. Follow the datasheet, IFS = VREF/1.32. VREF = 0.99V. But motor is hot when we set the value.

5. How to set Torque? I am not sure the relation between N.m and voltage. Can we set it by using the motor spec "PULL-OUT TORQUE=180gf-cm and PULL-IN TORQUE=150gf-cm"?

Regards,

Roy

  • Hi Roy

    Thanks for posting in this forum. 

    1. How can we measure the back-emf when motor was operating?

    It is not possible to measure BEMF explicitly because the driver outputs will be active while the stepper is running. With certain steppers, step mode setting and step rates observing xOUTx voltage may show superimposed BEMF sine wave. Generally speaking it is not possible to measure the BEMF explicitly. For stall detection we use indirect approach with smart tune ripple control STRC decay mode variable TOFF. The variations in TOFF is affected by BEMF. See this application note, https://www.ti.com/lit/an/slvaei3/slvaei3.pdf.

    2. We were using DRV8434AEVM to drive customer's motor. Customer's motor was moving up and down as picture showing. Why we met stall issue when motor moved up, but no stall issue when motor moved down. (We set the same VREF)

    It is possible the motor be over driven or stall threshold not setup correctly.

    3. When we used DRV8434AEVM, we produced the stall issue manually. But why start steps motor was still spin when stall occurred. It looks like that we didn't have stall protection, is it correct?

    The DRV8434A device provides stall detection and reporting only. The MCU controlling the DRV8434A should make a decision based on this reporting of stall. See Table 7-7. Fault Condition Summary in the current datasheet page-27.

    4. What does VREF voltage mean? Does it mean the current? May you help check if below equation is ok or not? The stepper motor spec shows the coil resistor is 8R and we use 12V. 

    12/8 = 1.5A(motor current). Because we used two phase and so one phase current should be 0.75A. Follow the datasheet, IFS = VREF/1.32. VREF = 0.99V. But motor is hot when we set the value.

    Yes, VREF is used for setting IFS (full-scale) current with TRQ_DAC = 100% setting. I have used similar stepper for headlight leveling applications commonly known as PL35L stepper motors. These are rated between 0.4 to 0.5 A IFS. The stepper drivers such as the DRV8889-Q1 or the DRV8434A are current mode drivers VM voltage does not affect the motor current as it will be regulated by the stepper driver. Usually the stepper manufacturer provides the IFS specification. It is not calculated like you described. Overdriving will heat the motor and reduce the motor life significantly. I'd recommend 400 mA for this motor. You can see the same type of motor in the stall detection application note I mentioned in #1.

    5. How to set Torque? I am not sure the relation between N.m and voltage. Can we set it by using the motor spec "PULL-OUT TORQUE=180gf-cm and PULL-IN TORQUE=150gf-cm"?

    Stepper motor output torque is a function of IFS setting. Motor vendor current specification will be for rated torque output. TRQ_DAC is used for reducing the current if needed. For example in hold mode to reduce the IFS such that the motor heat can be reduced if in hold torque mode for long period of time. Thank you.

    Regards, Murugavel 

  • Hi Murugavel,

    Thank you for your comments. Regarding to no. 5,

    1. I saw that DRV8434-Q1 doesn't have TRQ_DAC pin, but the other motor driver having like DRV8889-Q1.

    2. Can we input PWM pulse way into VREF to reduce the motor driver temp?

    Regards,

    Roy

  • Hi Roy,

    1. I saw that DRV8434-Q1 doesn't have TRQ_DAC pin, but the other motor driver having like DRV8889-Q1.

    This is correct. The DRV8889-Q1 has a SPI register for TRQ_DAC.

    2. Can we input PWM pulse way into VREF to reduce the motor driver temp?

    VREF input must be DC reference voltage. So a PWM based DAC, reference https://www.ti.com/lit/an/spraa88a/spraa88a.pdf?ts=1733238201002&ref_url=https%253A%252F%252Fwww.google.com%252F with an RC filter at the output can be used to vary the VREF voltage. So, yes, VREF can be set to a lower value during hold mode to reduce motor driver temp. Another easy approach, if you need only two levels of voltages, would be to add an additional resistor to GND from the VREF potential divider to reduce the VREF - see below. Thank you.

      

    Regards, Murugavel 

  • Hi Murugavel,

    On further question for EVM. When motor did the returning to zero action, we used the STALL signal to let MCU know the motor was back to point of original.

    In DRV8434 UI, there is clear button. When motor reached out to the point of original, the STALL became "H" and FAULT became "L". But when we pressed the clear, the STALL and FAULT weren't be reset. It could be reset when we let motor spin for a little and then click the clear.

    May you help comment it? Thank you.

    Regards,

    Roy

  • Hi Roy,

    The "Clear" button issues an nSLEEP reset pulse as described in the datasheet. 

    When motor did the returning to zero action, we used the STALL signal to let MCU know the motor was back to point of original.

    Could you please clarify? Were you referring to the HOME position of the indexer? Because STALL signal typically happens at the coil current zero crossings, do you use the STALL fault to interrupt the MCU and take immediate action with no time lag?

    In DRV8434 UI, there is clear button. When motor reached out to the point of original, the STALL became "H" and FAULT became "L". But when we pressed the clear, the STALL and FAULT weren't be reset. It could be reset when we let motor spin for a little and then click the clear.

    The UI may have a time lag in its response. So after clicking the clear button please wait for a sec or few until the fault is cleared. In my EVM setup this works as expected. Could you please check for the nSLEEP pulse on the header for the nSLEEP signal (single row header). Thank you.

    Regards, Murugavel