Tool/software:
Hi -
What is deglitch time on the ITRIP user-set current regulation?
I see tOCP is rated to 3uS typical / 5uS max. Also I see IPROPI typical with max SR is 10.5uS. Is ITRIP related to either of these values?
Thanks,
Tyler
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi -
What is deglitch time on the ITRIP user-set current regulation?
I see tOCP is rated to 3uS typical / 5uS max. Also I see IPROPI typical with max SR is 10.5uS. Is ITRIP related to either of these values?
Thanks,
Tyler
Hi Tyler,
Thanks for your question.
I am checking on this internally and will get back to you.
Thanks,
Ibinu
Hi ,
Thank you for your question.
ITRIP does not have deglitch time. ITRIP has tBLANK time only and it is "masking period" right after "DRIVE" starts.
regards
Shinya Morita
Hi Shinya,
Thanks for information. To clarify, when current goes beyond ITRIP user-set limit, the device will tBLANK time to recover (brake / decay) back below the user-set limit? So in this case it would be 5uS typical. Is that correct? Or am I misunderstanding?
Tyler
Hi Tyler,
brak/decay time is set by TOFF, not tBLANK.
tBLANK is ITRIP detection mask time. If we have such current peak during tBLANK, ITRIP will not be detected.
regards
Shinya
Hi Shinya,
Thank you for the explanation. The time period I am talking about is highlighted in yellow:
Can you help me understand how long the drive current can exceed ITRIP limit before the device moves into brake/decay mode? My customer had the following question, which is why I am asking: how long the current needs to stay above the trip limit to trigger the overcurrent regulation?
It still is not clear to me. My understanding is the time period I am looking for it neither tBLANK nor tOFF. Can you point me to which table in the datasheet defines this.
Regards,
Tyler
Hi Tyler,
Thank you for your questions. Once current level exceeds ITRIP level, output moves to Brake/decay immediately without intentional filter. It may have ??ns delay, but we can consider it is "immediately"
tOFF is period to restart "DRIVE". Here is my explanation. DRIVE"as A" starts and keep A/DRIVE until current level hit to ITRIP. As soon as hitting ITRIP, move to "B as Brake/decay". After tOFF period, it backs to A again.
Overcurrent protection is different topic. Not part of ITRIP.
regards
Shinya