Tool/software:
Hi,
I am using the "drv8434apwpr" in one of the design. Have a question on the stall detection.
The stall detection is not consistent. Initially, we had set the motor drive in "TorqueCount Mode" and checking the stall detection. But when the motor was getting STALL then the STL_REP signal was not becoming low. But some time it was becoming low as well (Not consistently we were detecting the stall)
Then we checked the "TRQ_CNT/STL_TH" pin voltage by setting the the mode to be in "TorqueCount Mode". We checked the voltage in motor ON condition (Voltage was around 90-100mV) and then during the stall condition (50-60mV). Then based on this observation, we have set a voltage of ~50mV at "TRQ_CNT/STL_TH" and changed the mode to "StallThreshold Mode". But we were having the STL_REP signal going Low (Stall detection) even when the motor was running normally. We tried change this voltage to 40mV to 75mV but the stall detection was happening even when motor was running normally. Any thoughts on this?
Then we wanted to do the learning process. But as per the procedure, the motor has to be run in steady state for 32 electrical cycle and 16 cycles in Stall condition. We wanted to understand 32 electrical cycle means what? One electrical cycle means one motor complete rotation?
Below is the snap shot of the motor spec for your reference.