This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8833C: find a lens motor driver solution

Part Number: DRV8833C
Other Parts Discussed in Thread: DRV8210, DRV8832

Tool/software:

Hi Sir,

My customer is looking for a lens motor driver shown as the below spec, could you please advise the solution? Thanks! 

Zoom: 190mA(typ), 320mA(max)
ND: 230mA(CLOSE), 230mA(OPEN)
SHT: 220mA(CLOSE), 200mA(OPEN)