Tool/software:
Hi,
I would like to use the DRV8214EVM to conduct experiments with very small motors (6 x 15 mm, diameter x length) to find out how good the current measurement/regulation is.
Since the motor inductance is very low, I would like to increase the PWM frequency to 100 kHz or 200 kHz to get a better current curve. There is a corresponding input field in the EVM GUI. However, if you try to enter a frequency other than the preset 25 kHz, the selection automatically jumps back to 25 kHz. How can I permanently set a higher value?
DRV821x_DRV823x-EVM-GUI/ver/2.0.2 (firmware version 0.29)
Thank you,
Matthias