Other Parts Discussed in Thread: DRV8434
Tool/software:
I have two questions for the experts.
1. Can the TRQ_CNT/STL_TH PIN of the DRV8434 be connected to the GPIO of the MCU without the need to connect to the GPIO of the MCU?
Is it possible to use a voltage value for this PIN as an action point for Torque count and stall threshold?
2.When nFAULT is changed from H to L or STR_REP is changed from L to H, how to change these two error signals back to the normal level after they are generated?
Is nSLEEP used to clear the error signal? Is it possible to clear the error signal by using the ENABLE pin?
3.When the nSLEEP of DRV8434 changes from H to L and the device enters SLEEP MODE, will the stator of the stepper motor still be excited?