Other Parts Discussed in Thread: DRV8462
Tool/software:
Hello. team
I'm making several attempts to turn the stepping motor at high speed using DVR8462, but there's a lot of degreasing and noise, so I'm inquiring to make sure I'm putting the parameters right.
The motor specifications are as follows, and we have confirmed that if we use a commercial driver with this motor, it is stably turned to 1500 rpm with low noise.
The picture below is a module equipped with DRV8462DDVR that I'm using.
Below are the settings to turn it to 600rpm. Near 600rpm, there's severe tremors and noise.
I have referred to the manual below.
If I did SS_THR 510Hz instead of 16Hz, it went back quietly.
I'm wondering if there is anything I misunderstand the manual, and please help me to adjust which parameters and how I should adjust it in order to raise it stably to 1500 rpm.