Other Parts Discussed in Thread: DRV8210
Tool/software:
Dear team,
i am using the replacement of Infenion IC part:- TLE75602ESDXUMA1 with DRV81602-Q1.
In infenion part the IN0 PINS has max limit of 7.6kohm of pin current(5.5v@0.75mA),So i kept 10kohm series resistor to that pin and connected microcontroller.
When i want to replace with TI IC the INx PINS has max limit of 7.6kohm of pin current(5.75v@0.75mA) as below picture but the recommendation is 4.7kohm as per below tables.
so what is the series resistor recommendation for this INX pins?
Best regards,
Navya.d