This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8316: Improving Graph Resolution for Monitoring PID Speed in Real-Time

Part Number: DRV8316

Tool/software:

Dear TI Experts,

In my project, I am monitoring the health of my PID controller by observing speed changes live using the graph view. I have a variable that updates every 1 millisecond, but when plotting this data on the graph, it appears to have a lower resolution than expected.

Is there an option to improve the resolution of the graph to better match the update rate of my variable? Or should I consider lowering the timer interrupt interval for better synchronization with the graph?

Thank you for your assistance!

* I update the speed in universal_motorcontrol_lab_f28002x (at systemVars.timerBase_1ms case 1) , using CCS 20,board f2800025c