Part Number: DRV3901-Q1
Tool/software:
Hello,
When debugging DRV3901Q, I found that the resistance of the explosion switch (load of DRV3901) was too low during initialization diagnosis (8.2.4.3.5): OFF_DIAG_STAT = 2h, Then I used a multimeter to measure the explosion switch, and the resistance was indeed 0.2 ohms (stable resistance, gradually decreasing from around 1 ohm from the measurement). Is this a problem with our selection? How can we adapt to the model we have chosen?
Additionally: 1. There is no clear description of DRV3901Q entering styandby mode;
2. MCU software reset (DRV3901Q without por), how to initialize drv3901, or in other words, what states can be used to determine that DRV3901Q is in standby mode.
3. What are the diagnostic parameters for the config register adjusted based on?