Tool/software:
What SIL/ASIL value does the MCT8316Z motor controller have?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We will get back to you by today.
Thanks and Best Regards
Venkatadri S
Hi
MCT8316Z is not safety certified under SIL/ASIL class.
What is your end equipment and can you provide more details?
Thanks and Best Regards
Venkatadri S
Good morning,
We would like to open and close a window with a motor controller for a BLDC motor.
There is a risk that a person will put their hand in the closing window.
This can be monitored with a sensor; in the event of jamming, the sensor switches, for example,
a relay which switches off the enable signal on the motor controller.
The sensor for monitoring must be SIL/ASIL compliant as it is a safety function.
As a result, the motor controller must also be SIL/ASIL compliant.
Are there other motor controllers for BLDC motors that are SUL/ASIL tested, e.g.
- DRV8316C
- MCT8316A
- MCF8316A
The BLDC motor runs at 24VDC and has a stall current of 6A.
Thanks and Best Regards
Bruno Rütsche
Hi Bruno Rütsche ,
These controllers are not SIL/ASIL tested.
Thanks and Best Regards
Venkatadri S