Tool/software:
Hi, I'd like to measure the efficiency of the motor inverter however I'm having trouble finding a possible connection point to measure the input DC voltage and current. I'm using the adapter and do not have a power supply to power the kit.
The current probes I'm using are clamp on and the differential voltage probes I'm using have grabber tips. Are there measurement points already on the board for me to do so or will I need to make modifications to do so?