This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8881: VREF and TRQ

Part Number: DRV8881


Tool/software:

Hi All,


I have a question about the DRV8881.

I have a DAC connected to VREF to dynamically change the current limit value.

If I change the VREF voltage, how long does it take for the output to stabilize?

Also, if I change TRQ, how long does it take for the output to stabilize?


Best Regards,
Ishiwata

  • Hi Ishiwata-san,

    Thanks for posting in this forum.

    I have a question about the DRV8881.

    I have a DAC connected to VREF to dynamically change the current limit value.

    If I change the VREF voltage, how long does it take for the output to stabilize?

    Internally to the device AVREF and BVREF are immediately updated at the Itrip comparator, so the changes would reflect immediately. It is fast enough to support microstepping indexing using an external MCU. Please see this application noteHigh Resolution Microstepping Driver.

    Also, if I change TRQ, how long does it take for the output to stabilize?

    Similar to the above the response will be immediate as well. May I know the purpose of this request? What is the desired response rate and why it is needed? Thank you.

    Regards, Murugavel 

  • Hi Murugavel-san,


    The customer is changing the current limit by dynamically changing VREF using a DAC.

    When the customer actually checked, there seemed to be no problem with TRQ, but the time it took for VREF to rise did not seem to be fast.

    The customer requested to know the specific time it takes for VREF to rise.

    Please tell us the specific time.


    Best Regards,
    Ishiwata

  • Hi Ishiwata-san,

    Thanks for checking with the customer and getting back to us. 

    We do not have a specification for this parameter for this device. We can do an example calculation based on the 256 microsteps example waveform in the application note which was implemented and tested to work with this device. See below snapshot. One half-wave is 32 ms. Within that half-wave the current level changes 512 steps using a sine table driven DAC driving the VREF. So VREF was updated every 32 / 512 =  62.5 μs with no issues. CH1 blue trace is real-time VREF change in this example.

    When the customer actually checked, there seemed to be no problem with TRQ, but the time it took for VREF to rise did not seem to be fast.

    Did the customer have any capacitor to GND on AREF and BREF? This can slow down the VREF voltage change rate. Also the settling time of the DAC used is important. The application note uses an MSP430 integrated DAC supports 1 μs settling time. 

    Please let us know what is the desired response time and purpose for it. Thank you.

    Regards, Murugavel