Tool/software:
We have been using the DRV8770EVM Evaluation Board as a pulse generator. Our setup consists of a Keysight Waveform Generator, with the + connected to INXA (both INHA and INLA shorted together) and the - connected to INXB (both INHB and INLB shorted together). The MODE pin is connected to GVDD. The MOTA output goes to the high side of our load and MOTB to the low side of our load.
We are using the external GVDD source and apply 18V to the board.
We are constantly grounding the INXB side, which is enabling the low side FET (connecting MOTB to GND), and we pulse the INXA side, which enables the high side FET to deliver the supply voltage to the load.
The waveform generator is outputting a single 0 to 5V square pulse. There are a wide array of pulse widths that we use, but they are on the order of milliseconds.
We have seen failures of the U1 component on 4 out of 5 of the DRV8770EVM boards that we have. The component has visible damage, near the center of the part.
Any ideas what could be causing the failures of the U1 component? Have you seen this in the past?
We noticed the logic input voltage is a function of GVDD, with a maximum voltage of GVDD +0.3V listed in the datasheet. If GVDD were not applied (0V) and our waveform generator outputted 5V to the INXA pins, could this cause damage?