Tool/software:
Hi team,
There is difference register setting about EN_STL between DRV8889 datasheet and DRV8889EVM-GUI.
Can you check which one is correct?


Regards,
Youhei MIYAOKA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
There is difference register setting about EN_STL between DRV8889 datasheet and DRV8889EVM-GUI.
Can you check which one is correct?


Regards,
Youhei MIYAOKA
Hi Miyaoka-san,
The CTRL5 bit #4 in the DRV8889EVM-GUI is used to Disable Stall detection which means DIS_STL = 0 enables the stall detection mode and DIS_STL = 1 disables that. However, the CTRL5 bit #4 in the DRV8889 datasheet is defined as EN_STL which is used to Enable stall detection. Therefore, EN_STL = 0 (equals to: DIS_STL = 1) means the stall detection is disabled, and EN_STL = 1 (equals to: DIS_STL = 0) means the stall detection is enabled. I hope this explanation made it clear for you. Thank you.
Best regards,
Mojtaba