Hi all,
I'd like some help on choosing a suitable motor driver / H-Bridge for a haptics application.
Basically it is a closed loop control application where brushed DC motors (Maxon) will be outfitted with quadrature encoders. The encoder values will then be read by a microprocessor which in turn control the motors via PWM. For a haptics application like this the motors will be resisting the user and basically stalling instead of driving.
What might be of importance too is that the motors must be able to switch directions really fast, < 1 ms (e.g. locking the mechanics in a specified position).
The motors we're looking at using are 60W - 100W at 25 Volts. I found the DRV8412, is that a good fit for this project?
Thanks for your help,
Anders