This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605L: Linux Driver for DRV2605L - doubts and integrating it with Raspberry Pi

Part Number: DRV2605L


Tool/software:

Good day dear TI experts,

I am looking for latest linux drivers for DRV2605L, which I can integrate with Raspberry Pi 5.

I checked the following links:

DRV260XSW-LINUX Driver or library | TI.com (Linux Driver)

CGit @ Texas Instruments - Open Source Git Repositories - git.TI.com/cgit (Android Driver)

From the above two links, it is clear that the driver is very old and Linux vs Android source code is also very different.

  1. So are there any latest driver for this?
  2. Is there any example or ref where the drivers are used on Raspberry pi?

Thank you,

Jitesh