Part Number: DRV8706-Q1
Tool/software:
Hi Expert,
In the project based on the DRV8706-Q1, the first batch of samples has entered the testing phase. Yesterday, we conducted preliminary experiments on the RE and CE functions. The test results showed that when the PWM duty cycle was 100%, the test passed successfully. However, when the duty cycle was not 100% (e.g., 50%, 60%, and a sweep from 20% to 80%), the test results failed. We performed tests at frequencies of 16kHz and 20kHz, and found that the duty cycle had a significant impact on the experimental results. How can I improve the EMC?
Thanks a lot!
Andy