This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8332-HT: DRV8332-HT RDS(on) value - incorrect Data sheet?

Part Number: DRV8332-HT


Tool/software:

Hello.

I need to know the RDS(on) value of the DRV8332-HT however the Data sheets does not make it clear what it is.

In Features it says that RDS(on) is 80mΩ

In Electrical Characteristics is says that RDS(on) is 260mΩ

and on the website in Product details --> Parameters, it says its 220mΩ !!

Can you please explain why these values are different and which is the correct value.

Thanks