This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8000-Q1: DVDD 3.3V

Part Number: DRV8000-Q1


Tool/software:

Hi team,

Could you please share your suggestions for below questions?

1. If the DVDD is 3.3V,what values should the RS_GND and RS_PVDD be?

2. Because OUTx output fault detection is related to the value of VDVDD. If 3.3V is used for fault detection, OUTX_PU and OUTY_PD both detect an open circuit, then the OUTX and OUTY values are always 1.65V, which is 2V below the OLP_REFL values. Does this indicate that the chip is consistently reporting the fault? Does the DRV8000-Q1 support 3.3V DVDD systems?

Thanks!

Regards,

Ivy