This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8329AEVM: DRV8329A Not Supported in SysConfig (Universal Lab Project)

Part Number: DRV8329AEVM
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hello,

I am using the F280025C LaunchPad with the DRV8329A inverter board for motor control. I am working with the Universal Motor Control Lab project in SysConfig. However, in the configuration folder, it shows that DRV8329A is not supported.

I have checked the available driver options in SysConfig, but I do not see DRV8329A listed. Could you please confirm whether the DRV8329A is supported in the Universal Lab project? If not, what would be the best approach to integrate this inverter board into the existing framework?

Any guidance on resolving this issue would be greatly appreciated.

Thank you!