Other Parts Discussed in Thread: DRV8962
Tool/software:
Hi,
I would like to drive a 100W 48V ( 2A nominal current, 5A peak ) motor with 62Vdc alimentation. I need a single full bridge or 2x half bridge in order to reverse the direction of rotation.
Could you suggest me a proper motor driver and configuration?
Is DRV8962 capable of such power?