Tool/software:
Hello,
We are currently usign the driver DRV8353FHRTAR controlled with a microcvontroller. We are using the hardaware version. We have found the follwing issues while using the driver.
- When enabling the driver, we have captured a dip in the nfault pin that triggers our error detection in the micronctroller, we would like to know why is triggering the nfault pin when enabling the driver during 2us.
- What is the reaction trime of the nFault pin from the point at which the errors arises until the pin is dirven low.
- Regarding the Hardware version, the OCP_MODE is configured by default to 01b? Is there any way to reconfigured it? If the mode 01b is used, the nfault pin should be driven low during 8ms? If not, where can we see this effect of the 8ms retry time?
Regards,
David