This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3901-Q1: NAD configuration and 3V3 SPI

Part Number: DRV3901-Q1


Tool/software:

Hello,

can the device be used with a 3.3 V SPI? From DS seems to be possible, can you confirm it? MOSI, nCS and CLK are received correctly. Only MISO need to be aligned to the microcontroller.

NAD address can be configured with a 3.3V pullup instead of 5V pullup? The check for the configuration is based on some voltage level o current measurement ?

Thank you.

BR,

Luca