This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Motor driver

Hello,

I cannot find a suitable part on below, can you pls confirm do we have a suitable driver?

8156.A3967[1].pdf

1)      Motor Magmotor S23-100

Continuous current: 5A

Peak current =15A

Const current=2A

 

Competitor part: MC33866

I cannot find a part that support up to peak current of 15A.

 

2)      Stepper motor 35F4K-05-020 Series 35000

Voltage=5VDC

Current=0.57A

Resistance/phrase= 8.8ohm

Inductance=13mH

 

I cannot find a driver that support stepper moter down to 4.75V

Competitor:A39673660.Magmotor S23-K-100.pdf7776.MC33886[1].pdf6787.Stepper motor 35F4K-05-020.pdf

  • Joy,

     

    1)  Have you looked at the DRV8432?  You can parallel connect the outputs to support the peak current you are needing.

    2)  You are correct, we currently don't have a device to support this.  What volume per year are you estimating for this application?