This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8462: Can I replace the DRV8462DDVR with DRV8262DDVR please advice .

Part Number: DRV8462
Other Parts Discussed in Thread: DRV8262

Tool/software:

Can I replace the DRV8462DDVR with DRV8262DDVR please advice .

  • Hi Chiina,

    The DRV8462 DDVR is a stepper motor driver with integrated indexer and other specific features to drive a stepper motor efficiently whereas the DRV8262 DDVR is a dual H-bridge driver primarily intended for driving two brushed DC motors. While the DRV8262 can be used for driving a stepper motor all the necessary indexing and drive logic must be custom developed in the driving MCU. Short answer is, you cannot interchange these two devices because of functionality differences. Thank you.

    Regards, Murugavel