Hi TI experts,
is it possible to measure back-emf at the phase, where just no current flows?
I saw the control in DRV8312, there /RESET and PWM can be set to low, make the phase up and down off.
In DRV8412 /RESET is not for single phase, but for A and B. So it is not possible here to make only one phase totally off.
That means a trapezoidal commutation, with based on back-emf, is not possible to be realized with DRV8412.
I know, for this kinda application DRV8312/DRV8301 is a good choice.
best regards,
Long