Part Number: DRV8234EVM
Tool/software:
has this been resolved?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brandon,
Thanks for the follow up.
Looks like the original thread got closed. David is out of office and should be able to look at this by early next week once he is back.
Thanks
Ibinu
Hi Brandon,
I reviewed the code in the linked thread and write to address 0x09 (CONFIG0) to set EN_OUT seems to be missing. Following the below steps I was able to get the OUT1 pin to go high with OUT2 being low:
Regards,
Joshua
Thank you for the response. I have one more question. When connecting to my ESP32-S3 via I2C, are there any shunts that should be removed from P1 main signal header? I have looked for guidance in the manual but have failed to find any.
Hi Brandon,
If connecting to an external MCU, remove all jumpers that are connected to the MSP430 (as shown in red box below). The A0 & A1 signals are tied to GND to set device addresses. The DRV_3V3 is suppling VCC pin on device with 3.3V and is supplied from the USB power.


Best,
David