Tool/software:
Hello,
I have a question regarding what the maximum temperatures the DRV110 can function or survive at. On the datasheet it says that the maximum operating range is from -40C to 150C, however, the storage temperatures range form -65C to 150C. Since the DRV110 is able to survive those storage temperatures, can it also operate or survive under -57C to 150C? Im especially more concerned about the low end of the temperature range as supposed to the high end. Please advise.
Thank you.
Manuel Valenzuela.