This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605L-Q1: Looking for 22Vp-p Haptic driver for Automotive application

Part Number: DRV2605L-Q1
Other Parts Discussed in Thread: DRV2510-Q1, DRV2511-Q1,

Tool/software:

I have one request related to the vibration module used our project.
It uses LRA (linear resonant actuator) as actuator for the haptic feedback function and we are looking for a driver IC with output voltage of 22.0 Vp-p (max) ​and output drive capability of 2.2Ap-p
Could you please suggest an automotive TI part to meet these requirements?
  • Hello,

    Thanks for reaching out.

    We have one automotive rated LRA driver which is DRV2605L-Q1 but this device can not achieve your output requirements. We do have two solenoid drivers though that are automotive rated (DRV2510-Q1 and DRV2511-Q1) which align closer with your output drive spec. 

    Regards,
    Sydney Northcutt