This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8889-Q1: SPI_ERROR

Part Number: DRV8889-Q1

Tool/software:

Dear team,

Is there any other fault indicated by SPI_ERROR register? D/S has 2 errors as examples.

Best regards,
Yuto

  • Hi Yuto - san, 

    Thank you for your question. The SPI-ERROR bit will indicate if any of the following criteria are not satisfied. 

    1-  The SCLK pin must be low when the nSCS pin goes low and when the nSCS pin goes high.

    2-  The nSCS pin should be taken high for at least 500 ns between frames.

    3-  Full 16 SCLK cycles must occur.

    4-  If the data word sent to SDI pin is less than 16 bits or more than 16 bits, a frame error occurs and the data word is ignored.

    5- The timing specifications should be followed. 

    Please let me know if you faced any challenge with the SPI to focus on the issue and find a solution. 

    Best regards, 

    Mojtaba