This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700: Flyback Configuration - Comparator

Part Number: DRV2700


Tool/software:

Hello,

I am currently looking at the DRV2700 in flyback configuration, specifically the schematic for DRV2700EVM-HV500. The documentation suggests that the MOSFET must be driven from a comparator, however the design uses OPA2376AIYZD, which is an op amp. I presume that this was chosen because an op amp was already being used in the active low pass filter for the PWM so the other channel was used for this. Can anyone confirm that U3A is definitely operating in open loop? i.e. VGate is only ever +5V or 0V?

Thanks.

  • Hi Toby,

    The OpAmp is being used as a comparator. A subtle piece of information is that the Rext = Vref = 1.35V. The Vpulldown voltage is being compared to 1.35V. Yes, U3A is operating in open loop and pulling the gate high (VDRV) or low (0V).