I am experimenting with the DVR8301-HC2 kit. I was able to work my through the basic GUI and then the Build steps with the code getting my motor to spin at the right steps. I started to add some code to the existing BLDC_Int project to read the potentiometer to set the speed. I started getting a driver fault as soon as I enable the motor. All the fault bits report "1". I've gone back to the stock code and I get the same result. I've done numerous power cycles to the same effect. So it looks like I did something to the DRV8301 driver. I am kind of baffled by all of the faults being set, unless this just means the driver chip has been damaged. Where should I start looking to confirm what happened?