This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8329EVM: Some about MCF8329 EVM question.

Part Number: MCF8329EVM


Tool/software:

Hi team,

My cuatomer use MCF8329EVM to do some test.

The product is Pump and spec is 48V@400W

But some question below,

1. The fan does not start smoothly, it makes a clicking sound and starts intermittently before starting again.

2. The startup current is about 2A. Is this normal? Can it be limited through the GUI?

3. IC working temp around 55C, Its no load condition. Is this normal?

4. Customer wants use the device to design 2.2KW. Can work?

Thanks