Tool/software:
Hello, I am currently trying to drive a 3-phase BLDC motor at 4100 RPM with a load using an EVM board at 12V after tuning. The current is around 7.7A, but the RPM is consistently maintained at around 3600. Could this issue be due to the speed KP or KI values? Or is it because the TI chip itself cannot produce enough torque?