Tool/software:
Hi team,
May I know that in the DRV8718-Q1 offline diagnosis, is the current source in the figure a common current source?
The customer used GH1/GH3/GH5/GH7, and the customer found that as long as there was one short circuit to ground on the high side of a load, the over-voltage faults of all four VDS were set 1. So they want to make sure that if the internal current source is common source.
Regards,
Ivy
Ivy