Tool/software:
When considering RPROPI values from DRV8243-Q1EVM, the ITRIP values will be in microamperes (µA). For a motor load current requirement of 3A, calculation using the maximum VTRIP value resulted in a very low RPROPI value. However, the recommended resistor value range is between 500 and 5000 ohms. Could you please help me for selecting RPROPI value for a 3A load output?
RPROPI taken from EVM,
VITRIP | 2.97 | V |
RIPROPI | 470 | ohm |
AIPROPI | 3075 | A |
ITRIP | 1.82667E-06 | A |
RPROPI Calculation for 3A ITRIP,
ITRIP | 3 | A |
AIPROPI | 3075 | A/A |
VTRIP | 2.97 | V |
RIPROPI | 0.000321951 | ohm |