This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8311: BLDC Motor Position Control

Part Number: DRV8311
Other Parts Discussed in Thread: AM62A7

Tool/software:

I would like to control the motor position using DRV8311 motor driver in AM62A7.

The application is gimbal motor control.

The motor rotation radius is 160 degrees. Please check if position control is possible using DRV8311. In the motor we are going to use, we can receive two analog hall sensor signals.