This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8329A: I2C clock speed

Part Number: MCT8329A


Tool/software:

Hi,

We are using the MCT8329A part in our project.

There are 3 ICs(MCT8329A) present in I2C bus and we are trying to read the speed from the status registers for every 500msec from those ICs. But sometimes we noticed that the speed is reading as 0.

We wanted to know the clock speed you recommend to keep? and frequency between the reads from each IC.

Also if we reduce clock speed do we still need to provide 100us delay between the bytes?

As we are using the STM32 there is no possibility of the providing the delay between each bytes at read time.

Please recommend the standard practice to follow when we read/write these ICs via I2C.

thanks,
Chandra