Tool/software:
I am considering purchasing one EVM boards for my application. I need to drive an inductive load (magnetic dipole antenna) using a 5-20Hz current waveform ON:OFF:-ON:OFF delivering a max current of 9.6A that have a slow ramp-up (~5ms) and a fast (1-5us) and linear current ramp-off (this waveform is also called a "sharkfin"). I wanted to know if I can use the EVM using the ENx and nSLEEP header pins, bypassing the USB and UART communication. I am using a Raspberry Pi 5 to do antenna and receiver array control and data acquisition. Suggestions are welcomed. Thanks