This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8329RRYEVM: Question about MOSFET in MCF8329RRYEVM

Part Number: MCF8329RRYEVM
Other Parts Discussed in Thread: MCF8329A-Q1, MCF8329A

Tool/software:

Dear TI experts,

My customer have a question about MOSFET in MCF8329RRYEVM.

I found that there are used CSD18536KTTT in each output of MCF8329A-Q1.

But my customer have limited PCB area, and CSD18536KTTT has large package than they expected.

So could you recommend that my customer can another MOSFET instead of CSD18536KTTT? (smaller than D2PAK package)

My customer should drive minimum 12V,70A BLDC motor assembly. (preferred 100A MOSFET.)

and one more question ;

Do it affect the value of Qg(Gate Charge Total) and Ciss(Input capacitance) to gate driver's performance?

If so, Could you check the recommended value(minimum or maximum) of these 2 parameters for the performance of gate driver?

Please check this issue. Thanks.

Best regards,

Chase