Tool/software:
Hi,
I want to use 2x DRV8162 for driving a full bridge.
The device requires some resistors for configuring mode, deadtime, etc.
Can I use a single resistor to configure, both devices? I want the deatime, mode, driving current and VDS monitoring to be the same in both hald bridges and would like to understand if I can save some components. The circuit diagram in the datasheet does not clarify whether the same component can be used. I assume there's a current source as drawn to know what resistor has been used. If that were the case then a resistor should be used for each driver.