This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8245-Q1: DRV8245

Part Number: DRV8245-Q1
Other Parts Discussed in Thread: DRV8145-Q1

Tool/software:

Hello,

I have load requirement of 5ohm, 2.2uF and 50mH with 16V battery voltage, DRV8245 is configured as independent half bridge and load is connected to load side only.

Can DRV8245 is capable of driving this load or is there any restriction?