This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMD18200QML: LMD18200QML related issues

Part Number: LMD18200QML

Tool/software:

Hello,

The customer recently conducted X-ray inspection on the received LMD18200-2D/883, and the inspection results are as follows:
Some components have a sealing width that is less than 25% of the design width. According to MIL-STD-883G method 2012.7 clause 3.10.2.2-e, the X-ray inspection is deemed unqualified.
Regarding the above results, the customer has raised the following two questions. Please help answer them. Thank you.

1. Why is the sealing width less than 25% of the design width?
2. Has the original factory conducted testing for the MIL-STD-883G method clause before leaving the factory? Do you have a test report?

Thanks!