Tool/software:
Hello,
Could you please confirm whether the phase comparator is a latching fault when set to fault mode in firmware?
Thank you, Keith
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
Could you please confirm whether the phase comparator is a latching fault when set to fault mode in firmware?
Thank you, Keith
Hi Keith,
Just want to confirm you mean if this bit is set to 1 you're asking whether it will be a latching fault or not correct?
I don't see anywhere in the datasheet that would indicate that this is a latching fault considering all the faults that are latching explicitly say so, regardless I'll check with systems.
Regards,
Yara
Hi Keith,
Apologies for the delay.
If the phase comparator fault is triggered then the following bits would report the fault
Although this wouldn't shutdown the gate driver, this fault would have to still be cleared using the CLR_FLT bit.
Regards,
Yara