This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8329A: MCT8329A - Maximum supported BLDC Motor RPM

Part Number: MCT8329A

Tool/software:

Hi,

I am using MCT8329A part for controlling my BLDC motor.

The Spec of the Motors are

Voltage: 14.8V
KV: 3650KV 
Configuration: 9N12P (12 Poles)

Since it is mentioned in datasheet that the maximum electrical frequency supported by MCT8329A is 3KHz, then according to the calculation of mechanical speed 

Mechanical Speed (RPM) = F(elec) * 60 / Pole pairs.

Given:

F (elec) = 3 KHz; Pole pairs = 6 then,


Maximum Mechanical speed = 30,000 RPM.

So by this can we confirm that MCT8329A supports a maximum of 30000 RPM? If not, please let me know what the maximum supported RPM is.