Part Number: DRV8329
Other Parts Discussed in Thread: DRV10975, DRV8334, , MCF8329A
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8329
Other Parts Discussed in Thread: DRV10975, DRV8334, , MCF8329A
Tool/software:
Hi Alex,
Thank you for your question! A member of the team will aim to get back to you by the end of the week.
Regards,
Anthony Lodi
Hello Alex,
Thank you for your question. To help us more precisely suggest a product for the constraints you already have, could you kindly respond to the following:
- What kind of motor algorithm do you plan on implementing? FOC? Trapezoidal? Sinusoidal?
- Do you plan on using an external microcontroller to implement the motor control algorithm?
- Are you considering single-shunt or three-shunt current sensing?
- Could you provide a value for peak motor current?
Cheers,
Joel A. Adejola
Hi Joel,
The motors that I plan on running will be sinusoidal commutation.
As for Microcontroller I am trying to stay away from using an MCU I am trying to use more control logic.
I was looking at the single shunt current sensing at the moment. Unless there is a safice option for three shunt current sensing.
Under no load max current draw for the biggest motor I am looking at running with be 2.5-3 A. But under full load I can reach anywhere from 20-30A.
Thanks,
Alex
Hey Alex,
Thank you for the clarifications. We will aim to get back to you next week with a recommendation part based on your requirements.
Cheers,
Joel
Hi Alex,
Check the suitability of MCF8329A. This is sensorless FOC control integrated gate driver, with abs max voltage rating of 65V. What is the load type in your application?
https://www.ti.com/product/MCF8329A
Regards,
Manu
Hi Manu,
Thank you for this information. I have checked over the MCF8329A and from the data sheet seems as if it could be a proper alternative. As for load type in our application, this will be kind of an across the board build. This drive should be able to support mechanical load as well as air movement load.
Thanks,
Alex Sanderson